Energy efficiency optimization
Recording and analyzing the heating requirements at Ettingen primary school
Ettingen wants to become a pioneer in energy efficiency, which is why the school complex needs to made more energy efficient. In order to determine the heating requirements of individual buildings, their consumption has been continuously monitored over an extended period of time. This data can then be used to adopt targeted measures.
Energy measurements in the school building's basement
Vorteile
-
Continuous and transparent recording of heating consumption
-
High data security
-
Monitoring of measured and energy values on the Memograph RSG45 display
-
Remote access via the intranet to the Memograph
RSG45 web server -
Reliable consumption data forms the basis of energy optimization
Customer requirements
The school complex requires drinking water, heating and electrical power for various buildings and facilities and, as part of an energy efficiency project, its consumption of heating energy is to be optimized. In order to plan and implement optimization measures on the basis of solid data, energy measurements must first be taken using a data logger for long-term storage.
The Endress+Hauser solution
The RSG45 with energy software calculates the cyclical thermal energy and heat output of the eight heating circuits using the relevant flow values and the corresponding supply and return temperatures. The system not only records heat consumption, but also heat generation, allowing users to compare these values and balance them against each other. In addition, it is possible to calculate the efficiency of the heat production on the basis of the fuels purchased and the thermal heat they generate.