Prova la ricerca per parole chiave, numero d'ordine, codice prodotto o numero di serie, per es. "CM442" o "Informazione tecnica"
Per avviare la ricerca, digitare almeno 2 caratteri.

A novel spin on beer testing

Are there bacteria in the fermenter that will spoil the beer? Laboratory analysis can answer this question, but it takes time. Now, a new system developed by Endress+Hauser enables on-site testing that is both quick and incredibly simple.

20.12.2024 Testo: Christine Böhringer Grafica: 3st kommunikation
Graphic of a PCR analysis system

Compared to water, beer is a safe drink. Its five percent alcohol content, slightly acidic pH value and near-zero oxygen content mean salmonella doesn’t stand a chance. But there are other bacteria and yeasts that have adapted to those conditions. Microorganisms that can spoil the beer may find their way in during the brewing process via ingredients, through contact with plant components or at the bottling stage – and compromise product quality over time. The result can be a beer that tastes or smells different, and may become cloudy, sour or unpalatable due to unpleasant aromas.

Breweries are keen on early detection of these impurities. Thus they run microbiological quality controls to prevent the spread of germs, the loss of entire batches or even product recalls. PCR laboratory analysis familiar from Covid-19 times represents the gold standard. “The lab procedure takes three and a half hours, using numerous machines in different rooms. Add to this the time needed to transport the sample, and two days can pass between extraction and result,” says Dr Nicholas Krohn, managing director of Endress+Hauser BioSense. The company is now helping brewers get there faster with a new PCR analysis system. With it they can test samples themselves, on site, for up to 18 beer-spoiling bacteria or yeasts. The small device is simple to operate and delivers results in under 90 minutes.

Laboratory expertise at the touch of a button

Centrifugal microfluidics is the core technology of this system. It allows minuscule amounts of liquid to be handled in the tiniest of spaces. “This means a single cartridge can carry out entire laboratory processes automatically at the touch of a button, without manual intervention for reagent handling. These lab-on-a-disc applications are already widespread in medical diagnostics. What we have done is transpose them into industrial process and laboratory automation,” says Nicholas Krohn. Another key element was an innovative sample concentration method developed by IST Innuscreen, an Endress+Hauser Group company. “The process doesn’t require centrifugation, filtration or flocculation, so it needs no special equipment or training. Any employee can prepare a sample for analysis in just a few simple steps,” Krohn is convinced.

How the on-site test works

A 100-milliliter sample of beer.

1.

Brewers use a special kit to draw a 100-milliliter sample of their beer and concentrate it using a two-step procedure they can easily perform themselves.

A single-use microfluidic cartridge shaped like a semi-circular disc.

2.

The sample is transferred to a single-use microfluidic cartridge shaped like a semi-circular disc, with all the necessary reagents inside. Each test run can be carried out with two cartridges.

Graphic of a PCR analysis system

3.

The cartridge goes into the processing unit. It runs a DNA or RNA extraction followed by a multiplex real-time PCR test, all at the touch of a button.

Graphic that shows spinning the cartridge subjects

4.

Rapidly spinning the cartridge subjects the contained liquid to centrifugal forces that steer it through internal channels connecting the reaction and analysis chambers.

Graphic of bacteria or types of yeast.

5.

Analysis algorithms interpret the results of the real-time PCR test, which are displayed on screen. It is thus possible to establish the presence of up to 18 bacteria or types of yeast.

Leggi argomenti simili

Download

Esplora altre risorse

document icon
Company magazine 'changes' 2/2024
The art of stable supply chains
download icon Download