Maintenance strategies such as preventive or predictive maintenance define how maintenance activities are executed. Condition monitoring provides the base information specialists needed to decide when action is actually required.
By leveraging digital enabled devices and secure connectivity, plant operators and maintenance teams can see asset condition during operation, either remotely or on the device. Having access to this information is what enables condition monitoring and enables earlier and better‑informed maintenance actions.
It does not define a maintenance strategy or replace maintenance expertise. Instead, it provides factual insight into asset health, based on real operating data, so maintenance actions can be triggered or planned for optimized maintenance work. While these insights help detect events or anomalies and support the decision-making process regarding when and how to intervene, the responsibility remains firmly with operators and maintenance professionals.
As such, condition monitoring is relevant both for maintenance and reliability teams seeking to improve decision-making, and for operations leaders assessing whether condition-based approaches can be applied reliably at scale.
Why condition monitoring matters in maintenance
Equipment health is becoming increasingly difficult to assess through periodic checks alone, that is where condition monitoring comes in. As assets become more complex and infrastructure more distributed, traditional inspection‑based approaches struggle to deliver insight in a timely fashion.
At the same time, maintenance teams often face limited resources and growing pressure to keep their plant running within a set budget. Therefore, teams focus their efforts on critical assets where it has the greatest impact. The results, non-critical assets often left unattended where issues quietly build up and remain unnoticed until they affect quality, availability, or safety.
By continuously collecting and contextualizing operating data, condition monitoring turns asset behavior into actionable insights. This enables a shift toward condition-based monitoring, where maintenance decisions are triggered by actual asset condition rather than fixed service intervals, allowing teams to intervene earlier and with greater confidence.
What is condition monitoring? Turning asset data into maintenance decisions
Condition monitoring makes asset condition visible during operation by observing measurable parameters over time. These parameters can include pressure, flow, temperature, level, or quality values, depending on the asset and application. The objective is to detect changes or abnormal behavior compared to normal operation, classify them according to NE107 status codes in order to plan maintenance activities effectively. It is not to predict failures far in advance, but to provide important insights.
At its core, condition monitoring digitizes asset health. Operating and sensor data is collected continuously or at regular intervals and made transparent, creating a reliable view of current asset condition. This visibility allows maintenance teams to recognize when behavior changes and when intervention may be required. Decisions remain human or rule-based, but they are grounded in objective condition data rather than assumptions or fixed schedules.
It works by establishing a baseline that represents normal asset behavior under real operating conditions. Deviations from this baseline indicate that something has changed. These changes may result from wear, fouling, drift, or process disturbances. Rather than relying on isolated signal values or alarms alone, condition monitoring focuses on trends and deviations that signal meaningful events.
Condition monitoring provides evidence for decisions; strategies define how those decisions are executed. It provides the transparency required for condition-based maintenance and supports strategies as preventive maintenance with insights. By basing decisions on actual asset behavior, teams can intervene earlier, avoid unnecessary work, and align maintenance actions more effectively with operational priorities.
Key elements of effective condition monitoring
Effective condition monitoring depends on the interaction of several core elements:
- Reliable field measurements. At the core is reliable field measurements that accurately reflect asset behavior. Without trustworthy data at the source, downstream insights lose meaning.
- Consistent data availability. Consistent data availability is equally important, whether data is accessed locally or remotely, it must be available when decisions need to be made.
- Clear indication of deviations. Clear identification and definition of deviations or abnormal states helps teams focus attention where it matters most.
- Understandable diagnostics. To ensure the correct reactive actions are taken, clear and understandable diagnostics are needed.
- Effective and secure connectivity. Connectivity underpins all these elements and ensure that condition monitoring can effectively scale.
Connectivity and remote access
Connectivity is what allows condition monitoring to scale beyond individual assets and support distributed operations. It can be implemented using different architectures depending on operational requirements. On‑premises setups are common when monitoring is closely integrated with existing automation systems. Cloud‑connected architectures add value for distributed or hard‑to‑access assets.
Connectivity enables near real-time monitoring no matter which architecture, depending on application and security requirements. Common industrial communication protocols such as HART, Profinet, Ethernet/IP and also IO-Link and Ethernet‑APL provide access to diagnostic and process data from field devices.
Edge devices and gateways often aggregate and preprocess data, enabling secure transmission while reducing load on central systems. A key requirement is secure coexistence with DCS and automation environments. Condition monitoring complements control systems by adding visibility without interfering with operation.
Why remote condition monitoring adds value
Many industrial assets are distributed, mobile, or difficult to access. In such cases, manual checks are inefficient and resource‑intensive.
Remote condition monitoring enables centralized visibility across assets through timely condition visibility across distributed assets, without the need for continuous asset visits. Deviations are detected earlier and with better context, allowing maintenance teams to plan interventions more effectively. This enables maintenance teams to plan interventions around planned downtime rather than reacting under pressure. This improves prioritization, reduces emergency work, and supports more predictable maintenance execution.
From condition monitoring to application‑specific monitoring
Condition monitoring provides a generic detection layer across assets. It identifies deviations and abnormal behavior regardless of industry or application.
For maintenance optimization, the next step is to relate this visibility to asset criticality and maintenance priorities. That turns generic condition data into actionable insight for better planning, prioritization, and intervention.
Example: Condition monitoring in water and wastewater applications
As one example, in water and wastewater applications, maintenance optimization is closely connected to process reliability, quality, and compliance. Condition monitoring makes process behavior visible, helps detect anomalies early, and provides the documented evidence needed for audit-proof operation. Across distributed infrastructure, this supports more targeted maintenance decisions and more reliable operations.
Condition monitoring in water and wastewater applications
Condition monitoring helps water and wastewater operators detect anomalies early, support targeted maintenance action, and maintain audit-ready records across distributed infrastructure. This strengthens reliability, quality, and compliance at the same time.
See how condition monitoring supports maintenance optimization in water and wastewater operations.