Food & Beverage Kit, Type Spoilage Bacteria Ident L
Simple, fast, and on-site detection of eight quality parameters indicating spoilage with our advanced testing kit.
©Endress+Hauser
©Endress+Hauser
©Endress+Hauser
Food & Beverage Kit for 10 reactions
Food & Beverage Kit for 10 reactions
Quality parameters
L. brevis, L. backii, L. rossiae, L. acetotolerans, L. lindneri P. damnosus horA gene & horC gene Sample types
Swab samples Water samples Beer samples (including dark beer) Samples non-alcoholic beer and shandy Enrichment samples Colonies from culture plate Analysis
Qualitative ("detected"/"not detected") Level ("low", "medium", "high")
The Kit enables the precise automated detection of quality parameters using qPCR and a microfluidic cartridge - and all of this conveniently on-site!
It contains the following components:
Sample preparation (10x)
Simple handling steps Fast sampling Enables analysis of many different sample types All necessary materials are included Detection Module (10x)
Microfluidic cartridge for fully automated DNA extraction and qPCR Operated in our Device BAB00
In addition to packaging as a Kit, we also offer the option of ordering the Detection Modules and individual workflow specific items for sample preparation in packs of 10 (see Ordering options).
Kit
Individual orders
10x Detection Module: BKB00-B06A3, replaces BKB00-B06A1 10x material for workflow with swab (colonies, swabs, enrichment): BPB00-E00A110x material for workflow for liquids (excluding dark beers and shandies): BPB00-D00A1Additional module for dark beers and shandies: BCB00-B00A4
Efficient workflow
Sustainable process optimisation that minimises losses due to unusable batches
On-site evaluation with minimal workload
Comprehensible process that does not rely on a laboratory
Clever process detective
Discover the problem areas of your process
Easier consistent
Maintaining brand image and customer satisfaction
Identify a variety of spoilage bacteria & resistance genes!
Do you have a specific application? We create customized solutions beyond the standard portfolio
Contenuti correlati
Novità, eventi e altro...
Argomenti correlati
Kit per alimenti e bevande, identificazione di Type Spoilage Bacteria Identification
Argomenti correlati
Food & Beverage Kit, Type Spoilage Screen
/
Disposal:
How should the Spoilage Bacteria Ident Kit be disposed of?
All components can be disposed of with household waste in accordance with local regulatory requirements. Accordingly, autoclaving is not necessary.
Single-use or reusable parts:
Are the materials, such as detection modules, reusable?
All components of the kit are designed for single use. However, Endress+Hauser is actively committed to environmental protection and works continuously to promote sustainable solutions.
Cross-contamination:
Is there cause for concern regarding possible cross-contamination?
Since the samples are analyzed in a closed system, there is no need to do so.
How do the Spoilage Bacteria Kits differ from one another?
“Spoilage Bacteria Ident” specifically identifies which beer-spoiling bacteria and resistance genes are present, while “Spoilage Bacteria Ident L” offers a broader scope of identification. “Spoilage Bacteria Screen,” on the other hand, indicates whether key groups of beer-spoiling bacteria and resistance genes are detectable. “Spoilage Bacteria Detect” combines identification and screening.
Accepted Sample Types: What types of samples can I test using the Spoilage Bacteria Ident kit?
Swab samples, liquid samples, and colonies. For more details, click here
Diamo valore alla tua privacy
Utilizziamo i cookie per migliorare la tua esperienza di navigazione, raccogliere dati statistici per ottimizzare la funzionalità del sito e fornire contenuti o annunci pubblicitari personalizzati.
Selezionando "Accetta tutti", ci autorizzi a utilizzare i cookie.
Per maggiori dettagli, consulta la nostra Politica sui cookie .
Personalizzare
Accetta solo l'essenziale
Accetta tutti